{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there a 120V control option card available for the ATV630 Process drives?
Issue:
Is there a 120V control option card available for the ATV630?

Product Line:
ATV630, ATV Process

Environment:
All

Cause:
N/A

Resolution:
A 120VAC input adapter card is not available for the process drives.
Consider an interposing relay for each digital input used.

Schneider Electric Global