Issue:
What Frame sizes are available for the Altivar 650 and Altivar 950 Process drive.
Product Line:
Altivar Process Drive (ATV650, ATV950)
Environment:
All serial numbers for Altivar 650 and Altivar 950
Cause:
N/A
Resolution:
The ATV650 drives are a version of the Altivar Process open drive (IP21) with a more robust housing for higher protection (IP55).
They come in 3 different Frame sizes described below.
Size A
What Frame sizes are available for the Altivar 650 and Altivar 950 Process drive.
Product Line:
Altivar Process Drive (ATV650, ATV950)
Environment:
All serial numbers for Altivar 650 and Altivar 950
Cause:
N/A
Resolution:
The ATV650 drives are a version of the Altivar Process open drive (IP21) with a more robust housing for higher protection (IP55).
They come in 3 different Frame sizes described below.
Size A
- 400/480Vac
- Includes the ATV630 and ATV930 from frame sizes 1 to 3
- 0.75 – 22kW (1 - 30hp)
- ATV650U07N4, ATV650U15N4, ATV650U22N4, ATV650U30N4, ATV650U40N4, ATV650U55N4, ATV650U75N4,
ATV650D11N4, ATV650D15N4, ATV650D18N4, ATV650D22N4
- 400/480Vac
- Includes the ATV630 and ATV930 frame size 4
- 30 – 45kW (40 - 60hp)
- ATV650D30N4, ATV650D37N4, ATV650D45N4,
- 400/480Vac
- Includes the ATV630 and ATV930 frame size 5
- 55 – 90kW (60 - 125hp)
- ATV650D55N4, ATV650D75N4, ATV650D90N4
Released for:Schneider Electric Global