{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV340 drives, do they have conduit kits?
Issue:
Do conduit kits come with the ATV340 drives?

Product Line:
ATV340 Altivar 340

Environment:
All

Cause:
Looking for an option for a conduit kit.

Resolution:
Conduit kits are not available for Frame sizes 1 thru 3.  Frame sizes 4 and 5 have integrated conduit kits.  Example of the frame size 4 and 5 with intergraded conduit kits is below.

ATV340 conduit kits

Schneider Electric Global