What are the temperature limit conditions for the Altivar Process Drive (IP21)?
Published date:
27 September 2019
Issue:
What are the temperature limit conditions for the Altivar Process Drive (IP21)?
Product Line:
Altivar 630 and Altivar 930 (IP21)
Environment:
All serial numbers for Altivar 630 and Altivar 930
Cause:
N/A
Resolution:
All “IP21 Products (except floor standing products) can be operated up to 50°C without de-rating and up to 60°C with de-rating.
The de-rating factor depends on the ambient temperature, the mounting position and the switching frequency (see applicable Installation Manual).
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.