{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do Altivar Process Drives have integrated Braking Transistors?

Article available in these languages: Spanish

Issue:
Altivar Process Drives integrated Braking Transistors.

Product Line:
Altivar Process Drives (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Resolution:
Not all Process Drives have braking transistors. Only the Altivar 900 series has integrated braking transistors.

ATV6xx
No Braking transistors available on the Altivar 6xx Process Drives

ATV9xx
Braking transistor availability:
Up to Size 4: Always integrated as a standard
Size 5 (IP21) + Size 7A: Available with or without braking transistor
Size 5 (IP55): Always integrated as a standard
Size 6, Size 7B and Drive Systems: Always without braking transistor (Braking unit is as an option available)

For Frame Sizes reference FAQ below
FA302753:What sizes are available for the Altivar 630 and Altivar 930 Process drive?

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)