{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What terminals are included in the Basic I/O Terminal Card for the Altivar 900 Process Drive?

Article available in these languages: Japanese

Issue:
What terminals are included in the Basic I/O Terminal Card for the altivar 930 process drive?

Product Line:
Altivar 900 Process Drive

Environment:
All serial numbers for Altivar 900 Process Drive

Cause:
N/A

Resolution:
Control ElectronicsATV900 Basic I/O-Terminal
  • 8 digital inputs
    • DI1, DI2...DI8
    • DI7 and DI8
      • Also frequency/pulse inputs
  • 2 STO (Safe Torque Off) – SIL3
    • STOA
    • STOB
  • 3 analog inputs
    • AI1
      • Configurable for voltage or current signal
      • Also used as temperature input (PTC probe)
      • Default as 0-10vdc
    • AI2
      • Configurable for voltage or (+/- voltage) signal
      • Default as +/- (0-10vdc)
    • AI3
      • Configurable for voltage or current signal
      • Also used as temperature input (PTC probe)
      • Default as 4-20mA
  • 3 relays
    • R1
      • 1 normally opened set of contacts and 1 normally closed set of contacts
    • R2
      • 1 normally opened set of contacts
    • R3
      • 1 normally opened set of contacts
  • 2 analog outputs
    • AQ1
    • AQ2
  • 1 digital output
    • DQ–
    • DQ+
      • Pulse output
  • 4 RJ45 connectors for communication
    • 1 Modbus RTU Port
    • 2 Modbus TCP/Ethernet IP Port
    • 1 Modbus HMI Port

Notes: The Altivar 600 Process Drive and removable connectors on its terminal card which is different from the Altivar 900 Process Drive. For the Altivar 900 Process Drive the complete board is removable

Schneider Electric Global