Will the displacement power factor on the ATV630 drive be better than the ATV61/ATV71 drives?
Published date:
11 January 2019
Issue:
Displacement power factor ratings on the ATV630 drive be better than the ATV61/ATV71 drives?
Product Line:
ATV630
Environment:
All
Cause:
Is the power factor more efficient than an ATV 61 and ATV71 drive
Resolution:
The displacement power factor for the ATV630 is similar to the ATV61.
See attachment for the current ATV630 and ATV930 displacement power factor ratings.