{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How to wire and setup 4-20mA signal for a Altivar Process Drive.
Issue:
Set up a 4-20mA Analog Signal on Altivar Process Drives.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
Altivar Process Drive

Resolution:
Wiring:
For wiring use AI3 and COM (AI3 is set to 4-20ma by default from the factory)
Can use the other analog inputs terminals on the drive as well (AI1, AI2, AI4, ...)

Setup:
[Complete settings] [Input/Output] [AI/AQ]


Schneider Electric Global

Attachment(s)
ATV600_Programming_Manual_EN_EAV64318_04 - Analog Input.pdf [2.34 MB]