{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I set the drive language on an ATV630/930 Process drive?
Issue:
Setting up the drive language on an ATV630/930 Process drive.

Product Line:
Process Drives

Environment:
All

Cause:
Need to modify the drive language used on the display

Resolution:
1. From the main menu, scroll down to menu 8 [My preferences].
2. Press OK to select 8.1 [Language].
3. Scroll to your desired language, press OK to select.