Issue:
Short Circuit (AIC) rating for Circuit Breakers inside the ATV660 Drive System.
Product Line:
ATV660, Process Drive System
Environment:
All
Cause:
NA
Resolution:
All Altivar 660 Process Drives include a circuit breaker as a disconnect device and
have a short-circuit rating of 100,000 A at up to 480 V.
Short Circuit (AIC) rating for Circuit Breakers inside the ATV660 Drive System.
Product Line:
ATV660, Process Drive System
Environment:
All
Cause:
NA
Resolution:
All Altivar 660 Process Drives include a circuit breaker as a disconnect device and
have a short-circuit rating of 100,000 A at up to 480 V.
Released for:Schneider Electric Global