Issue:
Altivar Process Drive with an SCF1 (Motor Short Circuit) Fault.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
Description
The drive is protected against short circuit between the phase output and phase and phase to the ground. When there is a short circuit, the inverter indicates the fault message SCF1
Causes
Remedies
Altivar Process Drive with an SCF1 (Motor Short Circuit) Fault.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
Description
The drive is protected against short circuit between the phase output and phase and phase to the ground. When there is a short circuit, the inverter indicates the fault message SCF1
Causes
- Short circuit at the inverter output.
- Short circuit or earth fault in the motor or motor cable.
- Earth fault.
Remedies
- Verify the cables connecting the drive to the motor, and the motor insulation (Megger test with the motor disconnected from the drive).
- Verify motor nameplate data has been entered properly in the drive and that an autotune has been completed (when motor is at room temperature).
- Go to Diagnostics menu and perform the IGBT test with motor when the motor is connected. If Not OK, then disconnect the motor and perform the IGBT test w/o motor.
- Reduce the switching frequency.
- Connect a load reactor (output choke) between the drive and the motor.
- Test the drive in an open loop mode (motor disconnected) to verify that the drive can operate without the error and generate balanced output voltages at several different speeds:
- Disconnect motor from drive and deactivate Output Phase Loss [Complete settings] [Error/Warning handling] [Output phase loss],
- Change Motor control type [Complete Settings,/Motor parameters to U/F VC 5pts
- run the drive with no motor connect.
- Check for balanced output voltages (phase to phase) at several speeds.
Released for:Schneider Electric Global