{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you change the Access Level on the Altivar Process Drive?
Issue:
Change the Access Level on the Altivar Process Drive.

Product line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
Altivar Process Drive

Cause:
Access Level set to Basic, and not all parameters are visible

Resolution:
[My preferences] -> [Access level]


From the Main Menu:
  1. Scroll down to My Preferences.  Push OK.
  2. Scroll down to Access Level.  Push OK.
  3. From here the Access level can be changed to Standard or Expert.