{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the ATV660 Harmonic filter IEEE519 compliant?
Issue:
IEEE519 compliance of the ATV660 Harmonic filter.

Product Line:
ATV660

Environment:
All

Cause:
Standard compliance required

Resolution:
An ATV660 ordered with a modification M09, Harmonic filter in field 09, complies with IEEE519.
See the attached file for supporting documentation.

Schneider Electric Global

Attachment(s)
ATV660 Harmonic filter.pdf [70.92 KB]