Issue:
User needs to convert a Float 32 register value into a decimal number
Product:
ION and Powerlogic Meters
Environment:
Arithmetic Conversion
Cause:
Some registers are stored as Float 32 values. In order to make sense of that value we have to convert that number to a decimal value.
Resolution:
Float 32 values will take 2 registers, if you check in the Register List.
- So, to start with convert the values separately in both the registers to Hexadecimal.
- Now, use the below link and use the value in the registers in ascending next to each
https://www.h-schmidt.net/FloatConverter/IEEE754.html
Below is an example of the process:
For Registers,
3000 - 5EF3
3001 - 4323
Input the hexadecimal box of the link as 5EF34323 to get the exact decimal values. 8.7644463E18
Attached document screenshot for further reference.
Released for:Schneider Electric Global