Issue
Is there a Connexium offer for fiber distances greater than 32 kilometers?
Product Line
Connexium TCSESM103F2LG0
SFP TCSEAAF1LFH00
Environment
Windows 10
Resolution
The Connexium TCSESM103F2LG0 switches and TCSEAAF1LFH00 Gigabit fiber SFP's can be used. These will support a distance of 24 to 72 Kilometers.
See attached documents for further information.
Is there a Connexium offer for fiber distances greater than 32 kilometers?
Product Line
Connexium TCSESM103F2LG0
SFP TCSEAAF1LFH00
Environment
Windows 10
Resolution
The Connexium TCSESM103F2LG0 switches and TCSEAAF1LFH00 Gigabit fiber SFP's can be used. These will support a distance of 24 to 72 Kilometers.
See attached documents for further information.
Released for:Schneider Electric Global