Issue:
Customer has the CFI2 fault on an Altivar Process Drive
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980, and APM)
Altivar Machine Drive (ATV340)
Environment:
All serial numbers
Cause:
N/A
Resolution:
The CFI2 is Configuration Transfer Error Fault.
Occurs when a configuration file can not be loaded to the device, or the configuration is not compatible with the drive.
Possible Causes:
Customer has the CFI2 fault on an Altivar Process Drive
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980, and APM)
Altivar Machine Drive (ATV340)
Environment:
All serial numbers
Cause:
N/A
Resolution:
The CFI2 is Configuration Transfer Error Fault.
Occurs when a configuration file can not be loaded to the device, or the configuration is not compatible with the drive.
Possible Causes:
- The was an unsuccessful or interrupted configuration file transfer.
- The stored configuration (HMI) was loaded from an different firmware. For example a file saved on a newer version drive can not be loaded into an older firmware version.
- Check firmware
- Firmware should be compatible on both drives
- Load a compatible configuration.
- Use SoMove to transfer configuration from another drive, or modify the saved SoMove configuration to match the drive being programmed.
- Perform a factory setting
- [Main Menu] [File Transfer] [Factory Settings]
Released for:Schneider Electric Global