Important Note!: For ATV600 drives only, the Ethernet IP option is a Communication Module it is not Embedded. When selecting option for Ethernet IP use the option for "Reference Frequency Via Fieldbus Module" [Com. Module]not [Embedded Ethernet]
Troubleshooting
Check Communication Map
[Display] [Communication map]
Check Command Channel
Command Register
Ref Freq Channel
Ref Freq
Disable FDR settings if not using a Faulty Device Replacement.
Check LEDs on the drive
The following FAQ describes the LEDs status for Ethernet IP Field-bus for the Altivar Process Drives