Issue:
Customer needs a graphic keypad for an ATV340?
Product Line:
ATV340
Environment:
Keypad display
Cause:
N/A
Resolution:
The ATV340 drive can use the Plain Text Display Terminal VW3A1113. It will be mounted directly to the front of the drive. It can also be remote mounted using part number VW3A1114, and one of the cables listed below.
The ATV340 drive can also use the Graphic Display Terminal VW3A1111 (also used on the Altivar Process Drives) which can be connected to the drive using the Remote mount kit (VW3A1112) and a cable
The cables to connect the display to the drive are:
1 Meter - VW3A1104R10
3 Meters - VW3A1104R30
5 Meters - VW3A1104R50
10 Meters - VW3A1104R100
NOTE: The drive does not come with either of these displays. They must be ordered separately.
NOTE: Only one display can be connected to the drive.
Customer needs a graphic keypad for an ATV340?
Product Line:
ATV340
Environment:
Keypad display
Cause:
N/A
Resolution:
The ATV340 drive can use the Plain Text Display Terminal VW3A1113. It will be mounted directly to the front of the drive. It can also be remote mounted using part number VW3A1114, and one of the cables listed below.
The ATV340 drive can also use the Graphic Display Terminal VW3A1111 (also used on the Altivar Process Drives) which can be connected to the drive using the Remote mount kit (VW3A1112) and a cable
The cables to connect the display to the drive are:
1 Meter - VW3A1104R10
3 Meters - VW3A1104R30
5 Meters - VW3A1104R50
10 Meters - VW3A1104R100
NOTE: The drive does not come with either of these displays. They must be ordered separately.
NOTE: Only one display can be connected to the drive.
Released for:Schneider Electric Global