{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to configure the SER2408/3200 device to work with the Generator Performance module in PME.

Issue
When attempting to assign I/O in the generator performance module, one is unable to locate all input assignments.

Product Line
Power Monitoring Expert 8.x
Data center Edition
Health Care Edition

Environment
Generator Performance module
Data center

Cause
Before the device can be properly configured in the Generator Performance Configuration Tool it must first be configured and added into PME properly.
After device data is logged into the database, you can assign device measurements using the Generator Performance Configuration Tool with EPSS Test Module.

Resolution
Please refer to page 238 of t he Applications modules configuration guide for instructions on configuring the SER hardware.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: