Issue:
ATV930 torque control over communications like Ethernet/IP
Product Line:
ATV930
Environment:
All
Cause:
Wants to write the torque reference over the network to control motor torque.
Resolution:
LTR address 8505 has to entered into the IO Scanner output table using Somove.
ATV930 torque control over communications like Ethernet/IP
Product Line:
ATV930
Environment:
All
Cause:
Wants to write the torque reference over the network to control motor torque.
Resolution:
LTR address 8505 has to entered into the IO Scanner output table using Somove.
Released for:Schneider Electric Global