{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do the Altivar 630/930 Series open style Drives include lugs for the input power and motor connections?
Issue:
Altivar 600/900 Series Drives lug inclusion

Product Line:
ATV600 and ATV900 series drives.

Environment:
All models, All serial numbers.

Cause:
Information unclear in current literature.

Resolution:
Lower horsepower ATV600/ATV900 series drives (Frame sizes 1 - 5)  have the terminal lugs built in to the housing of the drive.
For the larger horsepower (C11 and above: Frame sizes 6 and 7) lugs are not included. Bare terminals are available on the drive so that the customer can best choose the lugs to match the wiring they are using.
For Frame Size 6 only, there are recommended lugs that can be purchased separately. See this article for details.
Consult the ATV600 Installation manual or ATV900 Installation manual if you are not sure what the Frame Size is for a specific drive part number.

Schneider Electric Global