Issue:
ATV630 and ATV930 Process drives with blinking COM status led.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Com's status LED will blink when they connect the remote HMI display to the modbus port.
Resolution:
LED will flash when the fieldbus is active and communicating.
Released for:Schneider Electric Global