Issue:
ATV630 drives embedded Ethernet in I/O profile mode set up fault reset over network.
Product Line:
ATV630 or ATV930 in I/O Profile mode only
Environment:
All
Cause:
Wants to reset the faults over Ethernet using Bit 1 of the command word CMD.
Resolution:
With Profile set to I/O the assignment for fault reset will be C501 as fault reset being Bit 1 of the CMD with embedded Ethernet and I/O profile.
C501 means Bit 1 of the CMD 8501 will allow the faults to be reset over the embedded Ethernet network.
ATV630 drives embedded Ethernet in I/O profile mode set up fault reset over network.
Product Line:
ATV630 or ATV930 in I/O Profile mode only
Environment:
All
Cause:
Wants to reset the faults over Ethernet using Bit 1 of the command word CMD.
Resolution:
With Profile set to I/O the assignment for fault reset will be C501 as fault reset being Bit 1 of the CMD with embedded Ethernet and I/O profile.
C501 means Bit 1 of the CMD 8501 will allow the faults to be reset over the embedded Ethernet network.
Released for:Schneider Electric Global