Issue:
Viability of powering up a drive rated for 600V with 480V input and output 600V to the motor
Product Line:
Altivar drives
Environment:
All
Cause:
N/A
Resolution:
No. Such a configuration is a misapplication of the VFD.
The voltage supply and the motor voltage rating need to match. The only exception is a limited offering of ATV12 that accept 120Vac supply and produce 230Vac output.
Viability of powering up a drive rated for 600V with 480V input and output 600V to the motor
Product Line:
Altivar drives
Environment:
All
Cause:
N/A
Resolution:
No. Such a configuration is a misapplication of the VFD.
The voltage supply and the motor voltage rating need to match. The only exception is a limited offering of ATV12 that accept 120Vac supply and produce 230Vac output.
Released for:Schneider Electric Global