{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to setup a run status on the ATV630 and ATV930 Altivar Process drive?
Issue:
Setup a Run status on the ATV630 and ATV930

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
You can use any of your drive output relays for programming a run status. R1 is set by factory default to 'Operating State Fault'. Normally, R2 relay on the drive is an open set of internal contacts, and is (commonly) used for a run status, but it is not set for run status by factory default. The drive has 3 relays, and each of them are programmable for a run status assignment.
Just assign the specific relay to the function "Drive Running"

Procedure
Follow FAQ below on how to program relays:
FA245321:How are the R1, R2, and R3 relays programmed on the Altivar Process Drives?