{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
TeSys T Operating Modes and IO Logic
Issue:
What are the different TeSys T Operating modes? How are they different?

Product Line:
TeSys T Motor Management Controller

Environment:
North American Products

Cause:
Installation and Application


Resolution:
There are six main types of operating modes. Overload, independent, reverser, two-step, two-speed, and custom operating mode. Each has different wiring as well as specific behaviors for the TeSys T inputs and outputs.
See attached for more information.

Schneider Electric Global

Attachment(s)
Operating Modes (wiring and io logic).pdf [852.03 KB]