Issue:
Current consumption of the internal +24V DC power supply for the Altivar Process Drives ATV630/930
Product Line:
Altivar ATV630 and Altivar 930
Environment:
All
Cause:
Want to know if they can use the drives built in +24vdc power supply to power up a PLC card.
Resolution:
24V Output power supply for digital inputs and safety
function STO inputs O = +24 Vdc
Tolerance: minimum 20.4 Vdc, maximum 27 Vdc
Current: maximum 200 mA for both 24 Vdc terminals
Terminal protected against overload and short-circuit
In Sink Ext position, this supply is powered by external PLC supply
Current consumption of the internal +24V DC power supply for the Altivar Process Drives ATV630/930
Product Line:
Altivar ATV630 and Altivar 930
Environment:
All
Cause:
Want to know if they can use the drives built in +24vdc power supply to power up a PLC card.
Resolution:
24V Output power supply for digital inputs and safety
function STO inputs O = +24 Vdc
Tolerance: minimum 20.4 Vdc, maximum 27 Vdc
Current: maximum 200 mA for both 24 Vdc terminals
Terminal protected against overload and short-circuit
In Sink Ext position, this supply is powered by external PLC supply
Released for:Schneider Electric Global