Issue:
Altivar Process Drive setup to communicate over CanOpen
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
This FAQ will go over some basic settings to check. For a more detailed list of procedures on setting up the drive for CanOpen please reference the manuals attached.
EDS Files
- Programming with the Drive
Altivar Process Drive setup to communicate over CanOpen
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
This FAQ will go over some basic settings to check. For a more detailed list of procedures on setting up the drive for CanOpen please reference the manuals attached.
EDS Files
- Download and import CanOpen EDS files
- ATV600
- CANopen v1.1 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV600_CANopen_EDS_V1_1/
- CANopen v1.2 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV600_CANopen_EDS_V1_2/
- CANopen v1.3 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV600_CANopen_EDS_V1_3/
- CANopen v1.4 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV600_CANopen_EDS_V1_4/
- CANopen v1.5 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV600_CANopen_EDS_V1_5/
- CANopen v1.6 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV600_CANopen_V1_6/
- ATV900
- CANopen v1.1 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV900_CANopen_V1_1/
- CANopen v1.2 - VW3A36x8: https://www.se.com/ww/en/download/document/ATV900_CANopen_V1_2
- ATV600
- Programming with the Drive
- Program Communication Settings:
- [Communication] COM, [CANopen] CnO
- [CANopen Address] AdCo
- This is a read/write parameter. The parameter number is 6051 via Modbus access
- [CANopen Baudrate] bdCO
- This is a read/write parameter. The parameter number is 6053 via Modbus access.
- [CANopen Error] ErCO
- This is a read-only Parameter. The parameter number is 6056 via Modbus access..
- [CANopen Address] AdCo
- [Communication] COM, [CANopen] CnO
- Program Command Settings:
- [Complete settings] [Command and Reference]
- For command speed from Network, program:
- [Ref Freq 1 Config] Fr1 - Set to [CANopen] CAn
- [Ref 1B switching] rCb - Set to [Ref Freq Channel 1] Fr1
- [Control Mode] CHCF - Set to [Not separ.] SIM
- Video: Setting an Auto/Manual or Reference Switching on the Altivar Process Drives
- For command speed from Network, program:
- [Complete settings] [Command and Reference]
- Powercycle the drive
- [Parameters List] [Fieldbus] [Slot A - CanOpen]
- Configure
- CanOpen Address, Baud Rate & Error
- Configure
- Sending a command to the drive
- Configuration of the Drive for Operation in I/O Profile
- [Complete Settings] [Command and Reference] [Control Mode] - Set to IO
- Command Word - CanOpen Register 2037/2
Speed Reference Word - CanOpen Registers 2037/3 (Hz) or 2038/3 (rpm) - 16 bit word (Bit 0, 1, 2..... 15)
- Start/Stop for FWD command must turn on bit 0
- Write a 1 to start
- Write a 0 to stop
- Bit 1 to 15 are assignable like logic inputs
- Example: To assign a fault reset to bit 7 - [Fault reset] - Set to Cd07 (Reference Programming manual for more details)
- Using CIA402 (DriveCom Profile)
- Works with other assemblies
- [Complete Settings] [Command and Reference] [Control Mode] to [Not separ.] or [Separate]
- Command Word - CanOpen Register 2037/2
Speed Reference Word - CanOpen Registers 2037/3 (Hz) or 2038/3 (rpm) - No 16 bit word
- Start/Stop
- Sequence of values must be written to the drive
- 6, 7 and 15
- Toggle between 7 and 15 to start and stop or "RDY" to "RUN"
Released for:Schneider Electric Global