Issue:
Trying to set up a skip frequency on the ATV930
Product Line:
ATV930
Environment:
All
Cause:
Motor is making a noise when they ramping up and at 30hz.
Resolution:
Programming
Main Menu to complete settings
Next Generic Functions
Next Jump Frequency
Skip Freq set to 30hz for example
Skip Freq Hysteresis is 1hz
Drive will skip 29hz 30hz and 31 hz. as an example.
Trying to set up a skip frequency on the ATV930
Product Line:
ATV930
Environment:
All
Cause:
Motor is making a noise when they ramping up and at 30hz.
Resolution:
Programming
Main Menu to complete settings
Next Generic Functions
Next Jump Frequency
Skip Freq set to 30hz for example
Skip Freq Hysteresis is 1hz
Drive will skip 29hz 30hz and 31 hz. as an example.
Released for:Schneider Electric Global