{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you set up the analog input on the ATV630 and ATV930 for a current 0 to 20mA input?
Issue:
Analog input setup on the ATV630 and ATV930 for a current 0 to 20mA signal

Product Line:
ATV630 ATV930

Environment:
All

Cause:
Wants to set up AI1 for 0 to 20mA for speed control

Resolution:
Setting up AI1 as a 0 to 20mA input.

Using the HMI display

Go to the Main Menu
Go to the Complete settings
Go to the Inputs and outputs
Choose the 3rd function key black tab AI/AO
Go to the AI1 configuration
Go to AI1 type
Choose Current
Set AI1 min value to 0mA
Set AI1 Max value to 20mA.

Programming manual link

https://www.se.com/us/en/download/document/EAV64318/

Schneider Electric Global