{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I program an ATV630 Process Drive Relay R2 for a 3 second delay before energizing?
Issue:
Is it possible to program the ATV630 Process Drive Relay R2 for a 3 second delay before energizing

Product Line;
ATV630 ATV930

Environment:
All serial numbers

Cause:
Customer request.

Resolution:
Access: [Complete settings] [Input/Output] [Relay] [R2 configuration]
[R2 Delay time] r2d
R2 activation delay time has range  0...60,000 ms, so 3000 = 3 seconds.
The change in state takes effect once the configured time has elapsed, after the information becomes true.
The delay cannot be set for the [Operating State “Fault”] FLt assignment; and remains at 0.