Yes, there is new range of network braking units ATVRU75N4 (7.5kW unit) and ATVRD15N4 (15kW unit).
It is possible to combine up to 3 units in parallel. ATVR is compatible with ATV320, ATV340 and ATV900.
Manual (NVE88423) and sizing tool (NVE94856) can be downloaded from shopping kiosk.
It is possible to combine up to 3 units in parallel. ATVR is compatible with ATV320, ATV340 and ATV900.
Manual (NVE88423) and sizing tool (NVE94856) can be downloaded from shopping kiosk.
Released for:Schneider Electric Global