Issue:
Is ATV61 PRT power identify ratings setup similar to the ATV630?
Product Line:
ATV630
Environment:
All
Cause:
Wants to change the HP size in the field like the old ATV61 PTR parameter settings.
Resolution:
If you change the power board you will get prompted to choose.
However the standard drive does not have the same IP00 and IP20 settings like the ATV61 unless you are
Trained Field Services and have access to special access to the services tab in Somove..
So normally no its not a standard setting in the drive.
Is ATV61 PRT power identify ratings setup similar to the ATV630?
Product Line:
ATV630
Environment:
All
Cause:
Wants to change the HP size in the field like the old ATV61 PTR parameter settings.
Resolution:
If you change the power board you will get prompted to choose.
However the standard drive does not have the same IP00 and IP20 settings like the ATV61 unless you are
Trained Field Services and have access to special access to the services tab in Somove..
So normally no its not a standard setting in the drive.