Size of ATV650, 950 drives
S-A1 : 0.75kW to 5.5kW
S-A2 : 7.5kW to 11kW
S-A3 : 15kW to 22kW
S-B : 30kW to 45kW
S-C : 55kW to 75kW
Products sizeGland CAP
S-A1 : 0.75kW to 5.5kW
S-A2 : 7.5kW to 11kW
S-A3 : 15kW to 22kW
S-B : 30kW to 45kW
S-C : 55kW to 75kW
Products sizeGland CAP
ATV650 A11x ISO20
2x ISO25
ATV650 A21x ISO20
2x ISO25
ATV650 A31x ISO20
1x ISO32
1x ISO40
ATV650 B 1x ISO20
2x ISO40
ATV650 C 1x ISO20
2x ISO63
ATV950 A11x ISO20
2x ISO25
ATV950 A21x ISO20
2x ISO25
ATV950 A31x ISO20
1x ISO32
1x ISO40
ATV950 B1x ISO20
2x ISO40
ATV950 C 1x ISO20
2x ISO63
2x ISO63
Released for:Schneider Electric Global