{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV680- Do the input wires and motor wires come in the top or bottom?
Issue:
Input Wires come from the top or from the bottom on ATV680

Product Line:
ATV680

Environment:
Input Wiring and Motor Wiring

Cause:
n/a

Resolution:
According to the ATV680 Handbook (NHA37113) , the input power wiring and motor wiring can come from the top of the enclosure or from the bottom of the enclosure.  See page 95 of The ATV680 Handbook.

Schneider Electric Global

Attachment(s)
ATV680_Handbook_EN_NHA37113_02.pdf [7.46 MB]