Issue:
Running a smaller test motor on an ATV630 and ATV930 drive.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Set up drive for test on small power
Resolution:
You will need to set up the drive to run the smaller test motor.
Programming:
Main Menu
Complete settings:
Motor Parameters
Motor Control Type= Set to V/F 5 Points
In Simply Start menu set up your motor amps and HP to size of the test motor.
Be aware that you can run a smaller motor as long as the motor parameters in the drive will adjust low enough for the motor's specs.
Running a smaller test motor on an ATV630 and ATV930 drive.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Set up drive for test on small power
Resolution:
You will need to set up the drive to run the smaller test motor.
Programming:
Main Menu
Complete settings:
Motor Parameters
Motor Control Type= Set to V/F 5 Points
In Simply Start menu set up your motor amps and HP to size of the test motor.
Be aware that you can run a smaller motor as long as the motor parameters in the drive will adjust low enough for the motor's specs.
Released for:Schneider Electric Global