Issue:
Acceptable input voltage range for Altivar Process Drives ATV630/930
Product Line:
Process Drive
Environment:
All
Cause:
Supply Line Voltage
Resolution:
The line voltage tolerance is +10% and -15%.
Per the ATV600 and ATV900 Catalog, the range is as follows:
- 200 - 15%...240 + 10% three-phase for ATV…M3
- 380 - 15%...480 + 10% three-phase for ATV…N4
- 500 - 15%…690 + 10% three-phase for ATV….Y
Acceptable input voltage range for Altivar Process Drives ATV630/930
Product Line:
Process Drive
Environment:
All
Cause:
Supply Line Voltage
Resolution:
The line voltage tolerance is +10% and -15%.
Per the ATV600 and ATV900 Catalog, the range is as follows:
- 200 - 15%...240 + 10% three-phase for ATV…M3
- 380 - 15%...480 + 10% three-phase for ATV…N4
- 500 - 15%…690 + 10% three-phase for ATV….Y
Released for:Schneider Electric Global