{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What size bolts are needed to floor mount the NetShelter 4-post rack?
Issue:
A customer needs to know what size bolt will fit through the floor mounting holes in the rack.

Product Line:
NetShelter SX

Environment:
AR203A, AR204A, all serial numbers.

Cause:
There is no documentation as to the size of the floor mount holes.

Resolution:

A 5/8" diameter bolt (19 mm) will fit through the floor mount holes of the NetShelter 4-post rack.

Schneider Electric Global