{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives frame size five drives?
Issue:
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives

Product Line:
ATV600 and ATV900 drives frame size 6

Environment:
All

Cause:
Filter for bearing current reductions

Resolution:
The part number is VW3A5505 and its value of inductance is 183.2 uH

Schneider Electric Global

Attachment(s)
Altivar Process ATV900_VW3A5505.pdf [91.49 KB]