Issue:
Wants to program Jog Forward and Jog Reverse on the ATV630 and ATV930 drives.
Product Line:
Process Drive:
ATV600 series (ATV630, ATV650, ATV660, ATV680)
ATV900 series (ATV930, ATV950, ATV960, ATV980)
Environment:
All
Cause:
Application
Resolution:
The ATV600 series drives do not have a specific JOG function. Consider using a preset speed if required.
For the ATV900 series, you will need to wire and program per listed parameters below:
Under Complete Settings :
1. In the Command and Reference Menu > Reverse Disable = NO
...By Default in 2 Wire Control DI1 is Run Forward
**(note: by default DI2 is your Reverse Input)
2. In the Generic Functions Menu > JOG > JOG=DI5, JGF=10hz
When you enable DI1 and DI5 the motor will run forward at 10hz, when you enable DI2 and DI5 with DI1 Low, the motor will run reverse at 10hz. Always Stop by releasing DI1 or DI2 prior to switching directions.
Wants to program Jog Forward and Jog Reverse on the ATV630 and ATV930 drives.
Product Line:
Process Drive:
ATV600 series (ATV630, ATV650, ATV660, ATV680)
ATV900 series (ATV930, ATV950, ATV960, ATV980)
Environment:
All
Cause:
Application
Resolution:
The ATV600 series drives do not have a specific JOG function. Consider using a preset speed if required.
For the ATV900 series, you will need to wire and program per listed parameters below:
Under Complete Settings :
1. In the Command and Reference Menu > Reverse Disable = NO
...By Default in 2 Wire Control DI1 is Run Forward
**(note: by default DI2 is your Reverse Input)
2. In the Generic Functions Menu > JOG > JOG=DI5, JGF=10hz
When you enable DI1 and DI5 the motor will run forward at 10hz, when you enable DI2 and DI5 with DI1 Low, the motor will run reverse at 10hz. Always Stop by releasing DI1 or DI2 prior to switching directions.
Released for:Schneider Electric Global