{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can a Surge suppressor be installed on the output of a variable speed drive?
Issue:
Can a Surge suppressor be installed on the output of a VFD?

Product Line:
ATV12, ATV312, ATV32, ATV320, ATV61, ATV71, ATV630, ATV930

Environment:
All

Cause:
NA

Resolution:
It is not recommended to put Surge Suppressor on load side of VFD. The PWM output of the VFD will damage the Surge Suppressor components.

Schneider Electric Global