{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What would cause the drives HMI to show RDY when the remote start on logic input is being given?
Issue:
Drive state stays at RDY when the remote start on logic input is being given

Product Line:
Altivar drives.

Environment::
ATV12, ATV212, ATV312, ATV320, ATV61, ATV71, ATV630, ATV930

Cause:
Drive will not run.

Resolution:
a) Verify the run command at the drive terminals.
b) Measure voltage on the drive inputs to verify commands.
c) Verify the drive programming is set for terminal command.
d) Verify the drive programming for 2 wires or 3 wires control
e) Verify the command channel and command switching
f) Verify the drive is not in local mode control.

Schneider Electric Global