{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the input disconnector on ATV650C25N4F? Is there an input load-break switch (can disconnect nominal currents ) or disconnector?
It is INS630 (3-pole 630A switch disconnector) that is used as input switch-disconnector. It can be switched off under nominal current.

Schneider Electric Global