{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the parameters within the OFSinternal.xml file be adjusted to help improve the OFS performance?
Issue
Can the parameters within the OFSinternal.xml file be adjusted to help improve the OFS performance?

Product Line
OFS

Environment
Windows 10


Resolution
It is not recommended to make changes to the parameters listed in the OFSinternal.xml file.  Any changes made to the
parameters could make OFS imoperable.

If the OFS server is having perfomance issues (i.e., notification overrun being reported in the log, etc.), It is recommended
trying to tune the OFS network (Reference attached document).

Schneider Electric Global

Attachment(s)
OFS v3.40 Parameter Tuning_Rel1.0_Aug 2015.pdf [896.09 KB]