Issue:
PT/KTY/PTC specifications that can be used on the ATV630 process drive.
Resolution:
AI2-AI3 Sensor inputs I Software-configurable PT100/PT1000 or KTY84 or PTC or Water level
sensor
PT100
1 or 3 thermal sensors mounted in series (configurable by
software)
Sensor current: 5 mA
Range –20/200°C
Accuracy +/– 4°C for a temperature variation of 60°C
Released for:Schneider Electric Global