{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the power losses for ATV regen ATVRU75N4, RD15N4 ?
The power losses are :
- 12W in standby mode for both reference
- 346W at the continuous nominal power for the reference ATVRU75N4
- 381W at the continuous nominal power for the reference ATVRD15N4

To determine the losses according to the braking cycle, the curve is linear (0 power = 12W and 100% of power = 346W or 381W)

Schneider Electric Global