{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
My Process Drive with Modbus serial is not indicating when my cable is disconnected or no Modbus communication?
Issue:
My Process Drive with  Modbus serial is not indicating when my cable is disconnected or no Modbus communication?

Product Line:
Altivar Machines

Environment:
All models and serial numbers

Cause:
Not default program to the drive.

Resolution:
Drive has to be configured for command and/or reference from Modbus or drive sees this as monitoring only, will not trip if it's not there.  Under Error/Warning Handling > Fieldbus Monitoring > SLL - Response to Modbus Interruption is set to Freewheel