{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you monitor the status of the digital inputs on the ATV630 and ATV930 Process drives?
Issue:
Monitoring the status of the digital inputs on the Process drives

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Wants to monitor the status of logic input DI11

Resolution:


Address 5202 will show the status of the logic inputs.   if you want to monitor DI11 its bit 11 of the 5202 address.

"IL1I
IL1R"     Bit 0:     Value of LI1.
Bit 1:     Value of LI2.
Bit 2:     Value of LI3.
Bit 3:     Value of LI4.

Bit 4:     Value of LI5
Bit 5:     Value of LI6
Bit 6:     Reserved (= 0).
Bit 7:     Reserved (= 0).

Bit 8:     Reserved (= 0).
Bit 9:     Reserved (= 0).
Bit 10:   Reserved (= 0).
*   Bit 11:         Value of LI11

Bit 12:   Value of LI12
Bit 13:   Value of LI13
Bit 14:   Value of LI14
Bit 15:   Value of LI15