Issue:
Customer has a ATV630 and is controlling through Ethernet. It is setup in hand to run with the logic inputs. They want to be able to stop the drive while in Coms with a logic input. They do not want to use the STOA and/or STOB, because they do not want to have to power cycle the drive. He was wondering if he could assign a digital input to nst , and stop the drive, even while running totally ( start/stop and speed control) through Communications?
Product Line:
ATV630 drives
Environment:
Ethernet IP
Cause:
n/a
Resolution:
According to Engineering, to stop the drive with Comms, with a log input:
Use 3-wire control (TCC=3-wire control).
DI1 must be ON to run the drive, when you open it, you stop the drive (-->NST).
Customer has a ATV630 and is controlling through Ethernet. It is setup in hand to run with the logic inputs. They want to be able to stop the drive while in Coms with a logic input. They do not want to use the STOA and/or STOB, because they do not want to have to power cycle the drive. He was wondering if he could assign a digital input to nst , and stop the drive, even while running totally ( start/stop and speed control) through Communications?
Product Line:
ATV630 drives
Environment:
Ethernet IP
Cause:
n/a
Resolution:
According to Engineering, to stop the drive with Comms, with a log input:
Use 3-wire control (TCC=3-wire control).
DI1 must be ON to run the drive, when you open it, you stop the drive (-->NST).
Released for:Schneider Electric Global