{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the description of the returned Hex value in the #PLCQualStatus
Issue
What is the description of the returned Hex value in the #PLCQualStatus

Product Line
OFS

Environment
Windows 10


Resolution
The following is a description for the possible value returned by the '#PLCQualStatus' OFS variable.
  • 0x00C0 Communication with the device is correct.
  • 0x0040 No communication with the device since less than the configured Device Timeout.
  • 0x000C No communication with the device since the configured Device Timeout.
  • 0x0000  Device is not identified.
  • 0x0018 Device is inconsistent (SymbolFile differs from PLC application).

Schneider Electric Global